Summary
Introduction
CX series Configurator
Driver CX3
BootWizard
The scope of this manual is to show the functionalities of the
setup. When the user run the program on the screen the main window will open, like in the following picture:

With
this software is possible to install the CX3 Configurator software and it's USB driver.
There are two possible type of installations:
- Single installation
- Complete installation
In the single installation the user selects the software to install, from the list, clicks
on INSTALL button, and follows the instruction.
Otherwise, the user can select "All Software" and the setup will executes all the installations together.
This setup will install the application "Configurator CX3" on your computer.
The following pictures will guide you throughout the installation:




After the installation has finished, if the setup cannot find the directory where the software has been installed,.
It will ask you to insert the correct path with this popup:

The driver is necessary in order to establish a communication between the CPU of the SPIx and the computer.
The following pictures will guide you throughout the installation:



The BootWizard is being used to install and manage the firmware of the CX processor.
The following pictures will guide you throughout the installation:










The credit for this helper goes to Luca Alonzi.